Product Support Resources


                         
                         
                         

                        Power Factor Table Calculator

                         
                         

                        The Power Factor Table Calculator can be used to determine the capacitor kVAR required to improve PF of a single load or entire power system. Actual power factor, peak kilowatt demand and desired PF are required. The best source of this information is the monthly utility bill or other local monitoring equipment. A calculation of each months data for a 12 month period is recommended to determine the maximum kVAR required. To use the calculator click the link below.