Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


Product Support Resources


                         
                         
                         

                        Palm OS Selector Tool

                         
                         

                        The Drives Product Marketing group has developed Altistart® 01 softstart and Altivar® 31 AC drive selector tool software for your Palm OS equipped PDA device.

                        With a few simple inputs, such as phase, voltage, and HP/kW, a product is selected and the user can view detailed product information, including dimensions, list price, accessories where available, and more. Information for the entire family of products can accessed using navigation buttons.

                        The ATS01 selector provides information for each of the soft start families: N1, N2, U01N2 and the LY, as well as a Q&A section to assist in the selection process. The ATV31 selector provides information for the ATV31 drive offer.

                        Download the files

                        There is an application file for each of the two programs. Click the files below to download.

                        ATV31 AC drive selector tool files

                         
                         
                         
                         
                         

                        ATS01 soft start selector tool files

                         
                         
                         
                         
                         

                        In addition to the application program files, a runtime library must also be installed onto the Palm OS device.

                         
                         
                         
                         
                         

                        Installation is simple

                        Download all three files onto your computer hard disk into any directory. Double-click on each file to automatically install the selector software onto your PDA device during the next “Hotsync” of your device.