{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

Search FAQs

What is the expected life of my APC UPS VRLA battery?

Article available in these languages: Spanish

Issue:
What is the expected life of my APC UPS VRLA Battery?


Product Line:
All UPS Models


Environment:
All Three Phase and Single Phase UPS Models


Cause / Resolution:
Most APC batteries should last three to five years. There are many factors which affect Battery life including environment and number of discharges. Below are some guidelines to ensure optimum life expectancy:


1. Operating Temperature: The optimum operating temperature for a lead-acid battery is 20-25° C (68-77° F). Elevated temperature reduces longevity. As a guideline, every 8° C (15° F) rise in temperature will cut the battery life in half. A battery which would last for 4 years at 25° C (77° F), will only be good for 2 years if operated at 33° C (95° F). Keep in mind that the battery temperature inside your UPS will always be warmer than the ambient temperature of the location where the UPS is installed.

2. Battery Calibration and Deep Discharge: Only perform runtime calibrations on your UPS one or two times a year, if necessary. Some of our customers want to check their systems to verify that their runtime is sufficient. However, consistently performing these calibrations can significantly decrease the life expectancy of your APC battery.  It is also important to remember that a UPS is not designed for constant deep discharges. We do not recommend using your APC Smart-UPS/Back-UPS as a portable power supply that is repeatedly discharged/recharged (like on a portable equipment cart). These units are designed for emergency use during unexpected power outages or momentary loss of power.

3. Storage: Do not store APC batteries for extended periods of time. New batteries/units should be stored for no more than 6 months from date of purchase, as they ship from the factory at approximately 80% charge. After this period, the battery should be used or it will lose a great deal of its charge . It is not advisable to store batteries that have already been in use. Extended storage without periodic charging can result in shortened life expectancy and erratic battery performance.

Temperature also plays a large part in battery degradation during storage:

  • If the ambient temperature during storage is - 15°C to + 30°C (+ 5°F to + 86°F), perform a full recharge cycle at least every six months.
  • In environments where the ambient temperature is + 30°C to + 45°C (+ 86°F to + 113°F), perform a full recharge cycle at least every three months.


4. Load: As the load increases on your UPS, the runtime decreases. It is not recommended that the load exceed 80 percent of the UPS unit’s rated capacity. In the event of a power failure, a UPS loaded to full capacity will discharge the battery very quickly and there is a potential that the life expectancy of the battery will be significantly reduced.

5. Battery chemical reaction: As the VRLA (AGM) battery ages, a chemical reaction called "sulfation".
This leads to:

  • longer charging time than normal
  • excessive heat build-up leading to "boil out"
  • shorter running times between charges
  • dramatically shorter battery life

6. Battery replacement: since VRLA batteries end of life is five (5) years, it is always advisable to replace the UPS battery not longer than five (5) years to prevent the risk of possible hydrogen sulfide gas emission.

7. It is recommended to update the UPS firmware to the latest version to ensure all battery related improvements are available on the UPS system. Refer to FA164737 for updating the UPS firmware.

Schneider Electric USA

Explore more
Range:
Back-UPS ProAV Power Conditioners & Battery BackupsLine-RAPC ESAPC RS
Explore more
Range:
Back-UPS ProAV Power Conditioners & Battery BackupsLine-RAPC ESAPC RS
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.