Search FAQs
Can a QO2150, QO2175, QO2200, or QO2225SL be mounted in any location within a QO, single phase load center?
Issue:
Product Design Feature
Product Line:
QO load center and branch breakers
Resolution:
No, because of their physical size and the National Electrical Code (NEC) requirements for wire bending space, some restrictions apply regarding where these branch circuit breakers and subfeed lug kit can be mounted in the load center. Please refer to the instruction bulletin supplied with the branch circuit breaker or subfeed lug kit (link below) for clarification of the restrictions.
Instruction Bulletin
Product Design Feature
Product Line:
QO load center and branch breakers
Resolution:
No, because of their physical size and the National Electrical Code (NEC) requirements for wire bending space, some restrictions apply regarding where these branch circuit breakers and subfeed lug kit can be mounted in the load center. Please refer to the instruction bulletin supplied with the branch circuit breaker or subfeed lug kit (link below) for clarification of the restrictions.
Instruction Bulletin
Released for:Schneider Electric USA
Explore more
Product:
Explore more
Product: