Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image

 
 
 

Unity Pro Software Features

 
 

Unity Pro supports Modicon M340, Momentum, Premium, and Quantum PACs, as well as, new M580 hardware: Altivar Process Drive, X80 modules, HART and NOC communications, and Weighing modules

Unity Pro Conversion tools (from Concept, ProWorks, PL7 Pro) allow smooth continuity and migration from legacy PLC ranges to new PAC generations.

Productivity in design is boosted by an ability to reuse standardized objects and libraries, easy integration of field devices (FDT/DTM standard), compatibility with existing applications, powerful debug and simulation tools.

Cyber security features on M340 and Premium pACs include password protection and FTP/HTTP control.

Supporting Legacy LL984 programming in addition to the International Standard IEC61131-3: LL Ladder, SFC Sequential Function Chart (Grafcet), IL Instruction Logic, FBD Function Block Diagram, and ST Structured Text

A robust Concept/ProWORX converter

Support for Windows 7, Windows 8.a and Windows Server 2008

Unity Pro allows you to maintain and update installation without stopping process (CCOTF functions)

  • Create or remove variables without limitation
  • Create or modify multiple parts of the program in a single command
  • Add or remove PLC modules, or new Ethernet IO drops to update and extend your installation
  • Automatic update of SCADA application (Data Dictionary) without stopping communication

 

Contact your local Schneider Electric representative or authorized distributor for a FREE trial copy of Unity Pro v8.1 software.