Square D branded packaged drive products provides a robust adjustable speed drive solution for commercial and industrial applications. Included in our offer is the PowerGard(tm) 18-Pulse design for installations requiring strict adherence to IEEE 519 guidelines for harmonic mitigation. We combine rugged enclosure construction with a simply smart user interface, seismic qualification and wide connectivity network protocols to communicate with building automation systems creating an energy efficient, user friendly solution.
Telemecanique branded Altivar 61 drive defines ease of use for variable torque HVAC and pumping applications from 1 – 900 HP. Its evolutionary design will reduce installation and start-up time while offering reliable operation, simple diagnostics and energy efficiency. The ATV61 is plenum rated and qualified to the Semi-F47 standard with it’s ability for under voltage ride-thru.