Hotels


                 
                 
                 

                Success Stories

                 
                 

                Black Oak Casino Wins the Jackpot with Pelco’s Eudura Digital Security System

                SITUATION

                Black Oak Casino, a 165,000-square-foot facility, tucked into the Sierra Nevada Foothills of California’s Gold County needed a flexible security system that was easy to use, could provide maximum control and rapid response while meeting the stringent mandates of the governing Tribal Gaming agency.

                OBJECTIVES

                Improve Black Oak Casino’s security by giving them flexibility, ease of use, control and rapid response.

                SOLUTION

                Schneider Electric’s hotel solutions team installed the highly-sophisticated Endura video security system at Black Oak Casino. The Endura security solution is specifically designed for large scale facilities and uses an architectural approach to power through Ethernet networks delivering quality video, audio and control wherever - and whenever - it is needed.

                RESULTS

                Black Oaks is secure and the Casino is running smoothly. The Gaming Commissioner, Chairperson Delmar Geisdorff commented, "There is no comparison to the Endura security solution from Pelco/Schneider Electric when it comes to video quality, playback features and functionality, as well as the ability to immediately review video to resolve problems. Likewise, searching video is easy and, of course, we have achieved great savings when it comes to changing tapes and the costs associated with doing so"

                View the Full Success Story Here

                Moon Palace Golf & Spa Resort (Mexico) Saves Energy for More than 1,500 Rooms

                SITUATION

                Palace Resorts, a pioneer in all-inclusive resort facilities, operates several large scale resorts in Mexico. Their Moon Palace Golf & Spa Resort offers more than 1,500 rooms each with a private in-room spa and open-air balcony. Palace Resorts needed energy efficient solutions to improve overall energy consumption at their Moon Palace property.

                OBJECTIVE

                Deliver the finest guest comfort while reducing overall energy consumption.

                SOLUTION

                Schneider Electric’s hotel solutions engineering team created and implemented customized, integrated energy solutions for the Moon Palace Golf & Spa Resort.

                RESULTS

                Automation of HVAC and lighting management significantly reduced (and continues to reduce) Palace Resort’s energy consumption.
                Schneider Electric’s energy solutions worked because they offered a simple, user-friendly solution for managing HVAC and lighting.

                Palace Resorts saw immediate impact on energy consumption by managing room occupancy lighting and air energy consumption, and utilizing automatic detection of windows to control ventilation. The energy savings were so significant that Palace Resorts expanded the energy solutions to all five of their properties.

                View the Full Success Story Here

                  
                 

                 

                SE TV Cassia In-Room Energy Management System (EMS)


                Call 1-866-301-4272 or click here for more total Hotel Solutions information!