Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


News


        News Releases

        22/08/2016

        Schneider Electric announces dual communication protocol for PowerLogic PM5500 series meter

        ANDOVER, Mass., August 22, 2016 – Schneider Electric today announced BACnet IP protocol as an additional, standard feature for PowerLogic PM5500 power meters. These meters can now simultaneously communicate with building management and energy management systems using both BACnet and Modbus protocols. PM5500 meters are BTL tested to ensure seamless interoperability between products from any manufacturers, adherence to new building specifications and reduced risk of integration errors and associated costs in the field. The PM5500 meters are the first in the market to combine dual communications protocols and BTL certification.