Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


News


        News Releases

        09/02/2016

        Schneider Electric Introduces New Feature-Rich Feeder Meter for Utilities

        ANDOVER, Mass. – Feb. 9, 2016 – Schneider Electric, the global specialist in energy management and automation, today introduced the PowerLogic™ ION7400 three phase power meter, the newest addition to the PowerLogic portfolio. Ideally suited for feeder applications in electric utilities, the meter provides significant capabilities which include Class 0.2 revenue metering accuracy, Class S power quality, a utility-focused full color display and multi-protocol, multi-port communications. The meters also integrate seamlessly with StruxureWare™ Power Monitoring Expert (PME) analysis software or existing utility SCADA systems, can pinpoint disturbances by determining if they occurred upstream or downstream using patented disturbance direction detection (DDD), and can compensate for line loss, power and instrument transformer inaccuracies.