Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


News


        News Releases

        08/07/2013

        Schneider Electric Announces Availability of Conext Core XC-NA Inverter in North America

        PALATINE, Ill. – July 8, 2013 – Schneider Electric, a global specialist in energy management, announced today at Intersolar 2013 the availability of its Conext Core XC-NA™ inverter for North American customers. The Conext Core XC-NA Series is a new line of central inverters designed for high-efficiency and flexibility for any photovoltaic (PV) panel type and installation. The solution, designed to address the large commercial and centralized PV plants segments, has been enhanced to align with US required UL® certifications, listed to 1000 Vdc and comes with integral AC and DC switchgear which meets the requirements of National Electrical Code (NEC) 690.17