Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


News


        News Releases

        04/02/2013

        Schneider Electric expands its line of 22 mm push buttons with the Harmony XB7 monolithic range

        Raleigh, NC – February 4, 2013 – Schneider Electric, a global specialist in energy management, today announced the Harmony™ XB7 line of 22mm monolithic push buttons, switches and pilot lights. With a sleek design and robust features, the new XB7 line is well-suited for control applications that require durable units that are also compact in size and easy to install.