Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


News


        News Releases

        14/06/2011

        Schneider Electric Expands Altivar Line with the Altivar 212 and S-Flex Variable Speed Drives

        RALEIGH, NC – June 14, 2011 – Schneider Electric, a global specialist in energy management, today announced the new Altivar™ 212 variable speed drive and the S-Flex enclosed version, designed to provide OEMs and control panel builders with energy efficient and economical solutions for pump and fan applications.  The new AC drives adjust motor speed to the required flow of air or fluids, reducing energy costs by 50 percent. Engineered to provide additional cost savings, both the Alivar 212 and S-Flex feature electronic motor controls that reduce the mechanical stress on belts, piping and ductwork and eliminate valve or inlet guide vane maintenance.