Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image


News


News Releases

08/12/2010

Schneider Electric Introduces the New Magelis™ Smart + iPC, First Industrial PC with Microsoft® Windows XP® Pro Operating System

Schneider Electric today announced the Magelis™ Smart+ iPC, the first industrial PC with Microsoft® Windows XP® Pro that does not require maintenance or contain any rotating parts (no hard disk or fan). It also offers all of the openness associated with Windows XP® Pro. The Type 4X (IP65) touch screen shares the same 15" dimensions as the rest of the Magelis range. With its Intel® Celeron® M 1 GHz processor, 1 GB of RAM, and two Ethernet ports, Magelis Smart+ iPC offers great performance, and features a solid state drive (SSD) with Windows XP Pro.