Schneider Electric USA Website

Welcome to our website.

To view product availability in a specific country, select from the country list below. For Investor Relations, please visit our global site.

Choose another country or region

    • Default Alternative Text
      Medium speed, limited flexibility with coordinated motion.

      Medium Performance Packaging Machines

      A factory worker using a machine.

      Challenges

      A new era has already begun in the packaging industry. Today’s solutions require more flexible automation with intelligent electronic systems to meet customers changing demands and synchronize multiple axes. You need to increase the performance of your machines and reduce changeover time. You must also speed up time-to-market & reduce commissioning time.

      Increase performance

      Default Alternative Text
      • Solutions

        Dedicated to mid machines, requiring performances, this architecture  combines a CANopen network with Modicon M258 programmable controller, Altivar 32  / 71 variable speed drive or Lexium 32 servo drives and Magelis XBT GT display  unit. This implementation guarantees modularity, flexibility and openness of  your installation, due to the performance and efficiency of CANopen and Ethernet  IP
      • Value Proposition

        Machine Performance /  Flexibility

        • High level of adaptability with  M241 extension modules and the CANopen openness and Ethernet IP.
        • Perfect association drives ATV32 & servos drives  LMX32 (size, format, tools)
      • Differentiation

        Time to  market / One software - One connection
         
        • SoMachine combines in One single software the HMI and Controller programming  tools.
        • One connection to configure and to program
        • Easy and quick to connect variable speed drive and servo  drives on CANopen.
        • Pre-defined application function  blocks and libraries for easy programming.
      Side view of a packaging sealer machine.

      Packaging Machinery Solutions