Schneider Electric USA Website

Welcome to our website.

To view product availability in a specific country, select from the country list below. For Investor Relations, please visit our global site.

Choose another country or region

    • Default Alternative Text
      WHERE?

      Energy Savings Performance Contract ENABLE

      Gold american military pendant on an american flag
      The Energy Savings Performance Contract (ESPC) ENABLE provides a standardized and streamlined process for using ESPCs to implement energy efficiency and water conservation measures in Federal facilities smaller than 200,000 square feet.
      • Solutions

        By using the ESPC ENABLE, these facilities can realize energy and water savings within six months.

        Schneider Electric is a DOE Qualified ESCo and is listed on GSA Federal Supply Schedule 84, SIN 246-53 which contains a project financing offering that includes the ESPC ENABLE process.