• Default Alternative Text

    The Healthcare Guardian

    “To provide medicine to the highest order, we need buildings that perform to the highest order. We need electrical systems that are intelligent and that can help us identify potential issues prior to a failure.”

    Watch Video
  • Discover EcoStruxure™ Asset Advisor

    In healthcare environments, reliability of facility power systems takes on an added degree of importance. If the power goes out, critical research and the lives of patients are potentially at risk.

    Challenge

    Rochester-Medical-Center_Patient-IC-900x500
    • Maintaining a power infrastructure that spans 5 million square feet (464,500 square meters) of healthcare hospital and research space with limited resources.
    • Sending onsite staff to go out and physically measure, survey and perform preventive maintenance on over 26,000 pieces of equipment is costly and time intensive.

    Solution

    Rochester-Medical-Center_customerSEmonitor-IC-900x500
    • EcoStruxure™ Asset Advisor connects to and monitors the University of Rochester’s most critical electrical distribution assets via the cloud.
    • Event notifications are sent to facilities staff enabling them to gain advanced knowledge of potential problems.
    • Schneider Electric’s Service Bureau analyzes the asset performance data and provide actionable insights to help facility management deploy resources efficiently and help avoid equipment failure.

    Benefits

    • Allows for predictive, “condition-based” maintenance.
    • Nearly $1 million saved through early discovery of equipment problems- a 20 to 1 return on investment (ROI).
    • Peace of mind for facility management knowing equipment is continually being monitored.
    • University of Rochester Medical Center Case Study

      One of the USA’s premier academic healthcare organizations leverages EcoStruxure architecture to boost power system reliability.

      Read Full Case Study
      Default Alternative Text
      Default Alternative Text
      * required

      Sign up for Email? Learn about best practices, new solutions and offers.*