Schneider Electric USA Website

Welcome to our website.

To view product availability in a specific country, select from the country list below. For Investor Relations, please visit our global site.

Choose another country or region

    Intelligent PLC Control Devices


    Intelligent PLC Control (FAN2011996)


    The Modicon PLC family offers control solutions that are flexible, easy-to-use and more versatile. Led by the latest innovation – the M580 ePAC offering – which is the worlds first ethernet ePAC setting a new standard for ease of use and reliability.

    • Integrated Ethernet infrastructure
    • Open to third party devices supporting Modbus TCP and Ethernet IP
    • Embedded security features in compliance with IEC62443 standards and Achilles Level 2 certification