Schneider Electric USA Website

Welcome to our website.

To view product availability in a specific country, select from the country list below. For Investor Relations, please visit our global site.

Choose another country or region

    • Default Alternative Text

      Whole Home Surge Protection

      Whole Home Surge Protection

      Advanced appliance and electronics protection from surge damage

      Whole Home Surge Protection

      When surge protection is installed at the electrical panel, it helps protect all the devices in the home, including those that are not plugged into a surge plug strip (e.g. washers, dryers, stoves, refrigerators). Surges come from many different sources and can cause thousands of dollars in damage. The cost of surge damage can range from an immediate loss of electronics and appliances to long-term cumulative damage, shortening the life expectancy of expensive home possessions.

      Square D Surge Protective Devices have been engineered, designed, and developed based on decades of surge protection expertise and industry-leading technology, delivering innovation and performance in one standard package.

      Square D HEPD80

      The Square D™ Home Electronics Protective Device (HEPD80) is a compact and affordable surge suppressor designed for residential load centers. The HEPD80 reduces surges that might otherwise overwhelm plug strips and damage connected household equipment. It also provides surge suppression for important items that are not compatible with plug strips such as washers, dryers, refrigerators, stoves, heating and air conditioning equipment, and lighting.

      Surgebreaker Plus

      The Surgelogic™ Surgebreaker™ Plus Surge Protective Device protects the entire home from high-energy power surges and low-energy repetitive surges by delivering surge suppression. Surgebreaker Plus surpasses competition through sophisticated modular technology, compact footprint, ease of installation, and easy retrofit capabilities.

      Whole Home Surge protection

      QO and Homeline Surgebreaker

      The QO™ and Homeline™ Surgebreaker is a plug-in surge protective device (SPD) that is installed internally within the load center and is designed to protect the home's electrical system and hard-wired appliances from surges. Installing a Square D Surgebreaker provides critical surge protection against surges that may overload ordinary surge strips.

      Today's picks

      • Default Alternative Text Discover Juno
      • Default Alternative Text Get inspired Ideas and creative tips room by room