Technical FAQs

Ask a Question

Video: How can you program the ATV312 to use the local knob or remote HMI dial for speed control and terminal control for starting and stopping?
Issue: Need to use a dry contact for 2 wire control to start and stop the drive but use the local knob to control the speed on the ATV312 drive. Product...
How many circuit breakers can be daisy chained to an IFE ethernet gateway?
Product Line: Circuit breakers on a single modbus network Resolution: You can connect up to 13 breakers to one IFE/Gateway.  One connects directly...
Parts needed to upgrade a Masterpact NW breaker from a Micrologic 3.0 or 5.0 to the 3.0A 5.0P 6.0P 5.0H or 6.0H trip units
Inquiry: Which parts are needed to upgrade a Masterpact NW breaker from a standard trip unit to a Micrologic 3.0A 5.0P 6.0P 5.0H or 6.0H? Product...
Video: How is the Clock set in a M221 Controller?
Attached is a video on setting the clock. There are 2 ways to set the clock manually or Automatic using the PC clock.  
What is the function of an SDX switch?
Issue: What is the function of the SDX relay module for Powerpact H J and L circuit breakers? Product Line: Powerpact H, J, and L circuit breakers...
How should thermal scans of circuit breakers be used?
Product Line: All MCCB and Masterpact circuit breakers Cause: IR scans often contain images and verbiage indicating problems with the installation...
Video: Setting an Auto/Manual or Reference Switching on the Altivar Process Drives?
Issue: Video: Setting an Auto/Manual or Reference Switching on the Altivar Process Drives? Product Line: Altivar Process 600 and 900 Drives Environment:...
Video: Firmware upgrade on a PM800, PM5XXX, CM4000/T, CM3000 and CM2000 series meters using DLF-3000
Issue A user would like to upgrade the firmware on a PM800, PM5000, CM3000 and CM4000 series (Powerlogic) meter. Product Line PM800 series power meter...
What are the basic troubleshooting steps for the Back-UPS RS model BR1000G?
Issue: What are the basic troubleshooting steps for the Back-UPS RS model BR1000G? Product Line: APC Back-UPS RS Environment:  BR1000G, All Serial...
Why might the LEDs on my Back-UPS or Smart-UPS SC be flashing?
Issue: Flashing LED lights on Back-UPS Pro, Back-UPS Pro USB, Back-UPS LS, and Smart-UPS SC: causes and definitions Product Line: Back-UPS Pro, Back-UPS...
Results 1 - 10 of 100