Technical FAQs

Ask a Question

What is the maximum breaker that can be installed in the QONQ42MS400?
Issue: Need to know the maximum amperage of breaker that can be installed. Product Line: QO Panels Environment: QO Panels Cause: Breaker sizing Resolution: ...
Video: Do the H- and J-frame Powerpact breakers come with the extended handle?
Issue: Do the H and J frame Powerpact breakers come with the extended handle? Product Line: H-frame and J-frame Environment: Molded Case Circuit Brekaers...
Is there a 208Vac, 240Vac or 277Vac shunt trip for the J frame breaker?
Issue: Is there a 208 V, 277 V or 240 V shunt trip for the PowerPact J-frame breaker? Product Line: PowerPact J Frame Environment: This applies to...
What is the padlock attachment for a KA or KAL type circuit breaker?
Issue:   Is there a padlock attachment for the KA, KAL, KH or KHL frame circuit breakers? Product Line: Molded case circuit breakers Environment:...
Default administrator authentication phrase used by PowerChute Network Shutdown to communicate with the Network Management Card
Issue: What is the default administrator authentication phrase used by PowerChute Network Shutdown to communicate with the Network Management Card?...
Do we have a lug for the Powerpact P Frame I-Line breaker that will accept (3) 600 kcmil cable?
Issue: What is the part number for a lug to accept 3 - 600KCMIL cable for the Powerpact P frame I-line constructed breaker? Product Line: Circuit...
What is the catalog number for a sensor plug for a Powerpact or Masterpact breaker? Installation notes provided.
Issue:   Looking for sensor plug part number to adjust amperage on Powerpact or Masterpact breaker Product Line: Circuit Breakers Environment: Applies...
Motor operated P frame; which electrical accessories are available?
Title:   Motor operated P frame; which electrical accessories are available? Product Line: Molded case circuit breakers Environment: Powerpact P frame...
What is the suffix -1680 on the PAF361600DC-1680 breaker?
Issue:   What does the 1680 suffix indicate on a PAF frame breaker?   Product Line: Circuit Breakers Environment: Electrical Distribution Equipment...
Video: How to Wire a Square D™ 9013 Power Pressure Switch
Product Line: Square D™ 9013 Power Pressure Switches Resolution: When looking directly at the switch you should see four terminals going from left...
Results 1 - 10 of 100