Technical FAQs

Ask a Question

What is the maximum amperage branch circuit that can be installed in an NF Panelboard?

Issue:
What is the maximum amperage branch circuit that can be installed in an NF Panelboard?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
A 125 amp maximum branch circuit breaker can be installed in an NF Panelboard.


CTA-ID : 2003679
Was this helpful?
What can we do to improve the information ?