Technical FAQs

Ask a Question

Does a UT4R2352T include lugs?

Yes, the main lugs and branch lugs are included. The main lugs will accept (1) #1/0 AWG - 500 kcmil, aluminum or copper conductors, per phase and neutral. The branch lugs will accept (1) #8 AWG - 250 kcmil, aluminum or copper conductors, per phase and neutral.


CTA-ID : 2003474
Was this helpful?
What can we do to improve the information ?