Technical FAQs

Ask a Question

Can an XVBC21 be mounted directly to a panel?

Issue:
Can an XVBC21 be mounted directly to a panel?                 

Product Line:
Harmony Tower Lights

Environment:
All Products

Cause:
Product Features

Resolution:
Yes. You have remove terminal strip and drill or knock out 2 holes in base as indicated in the instructions. These are partly done from factory. This will allow the unit to be direct mounted. Gasket is provided with base unit for this purpose.


CTA-ID : 2001138
Was this helpful?
What can we do to improve the information ?