Technical FAQs

Ask a Question

What are the rail and deadfront extensions required to mount an NQOD442L225 or NQOD442L225CU in an MH50 or MH50WP?

The following parts will be required per panel and can only be mounted at the mains end:

(2) 80110-288-05 15`` rail extensions
(1) 80110-291-04 MLO cover 15`` extension
(2) 80110-289-01 Deadfront mtg brackets
(2) 80025-067-01 Deadfront screws
(4) 21590-17081 Rail extension screws

Revised 3/25/04






CTA-ID : 2004219
Was this helpful?
What can we do to improve the information ?