Technical FAQs

Ask a Question

Are main and branch circuit breakers supplied with the QO48M30DFGPW1 Pre-Wired Generator Panel?

Yes, both main breakers and branch breakers are provided in this device. Two QO230 circuit breakers are mechanically interlocked as the main breakers. Branch circuit breakers include (2) QO120 and (4) QOT1515, providing (2) 20 ampere and (4) 15 ampere branch circuits.


CTA-ID : 2003665
Was this helpful?
What can we do to improve the information ?