Technical FAQs

Ask a Question

Does the 9991SDH1 come with holes for push buttons?

The 9991SDH1 is provided with three closing plates which cover the holes and can be replaced with 30mm push button operators. The enclosure is also supplied with external overload reset operator.


CTA-ID : 2003659
Was this helpful?
What can we do to improve the information ?