Technical FAQs

Ask a Question

Is there a 400 ampere EZM branch device, 1 Phase In / 1 Phase Out?

Yes, order EZML111400 for a 1 gang device. Order EZML112400 for a two gang device. These devices are supplied with DJM tenant breakers, which can be adjusted from 160A - 400A.


CTA-ID : 2004200
Was this helpful?
What can we do to improve the information ?