Technical FAQs

Ask a Question

Can a KAL36250 be mounted in a KA225A circuit breaker enclosure?

No, the KA225A is restricted to 225 ampere maximum, due to wire bending space restrictions. Consider using IK250AWK.


CTA-ID : 2004213
Was this helpful?
What can we do to improve the information ?