Technical FAQs

Ask a Question

Can a KAL36250(250amp Max) breaker, be mounted in a KA225AWK circuit breaker enclosure?

Issue:
Product design features

Product Line:
Circuit breaker enclosures

Environment;
Circuit breaker

Cause:
Application

Resolution:
No, the KA225AWK is restricted to 225 ampere maximum, due to wire bending space restrictions. Consider using IK250AWK.


CTA-ID : 2004214
Was this helpful?
What can we do to improve the information ?