Technical FAQs

Ask a Question

Can a KAL36250 be mounted in a KA225DS circuit breaker enclosure?

No, the KA225DS is restricted to 225 ampere maximum, due to wire bending space restrictions. Consider using IK250DS.


CTA-ID : 2004212
Was this helpful?
What can we do to improve the information ?