Technical FAQs

Ask a Question

Are knockouts provided in a LA400R circuit breaker enclosure?

Knockouts are provided in the lower sidewalls, lower backwall and lower endwall. A concentric knockout pattern for 1.5``, 2``, 2.5``, 3`` or 3.5`` conduit is provided in each lower sidewall and lower backwall. A concentric knockout pattern for 1.5``, 2``, 2.5``, 3`` or 3.5`` conduit and two concentric knockout patterns for 1.5``, 2``, 2.5`` or 3`` conduit are provided in the bottom endwall. The top endwall is blank.


CTA-ID : 2003918
Was this helpful?
What can we do to improve the information ?