Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a H323A, safety switch?

The Equipment Ground Kit is factory installed in this switch (F design series). Two ground lugs are provided, each accepting (1) #12 - 1/0 aluminum or (1) #14 - 1/0 copper ground conductor.


CTA-ID : 2003903
Was this helpful?
What can we do to improve the information ?