Technical FAQs

Ask a Question

Can the SDSB1175C Surgebreaker Plus be used in parallel disconnect applications.

Yes, a properly installed Surgebreaker Plus will protect two main breaker load centers wire in parallel from a single meter socket if both load centers are each within five (5) feet of the meter socket. However, the branch circuit breakers that surge sensitive devices and electronics are connected to should be zoned within the panel that contains the Surgebreaker Plus.


CTA-ID : 2004199
Was this helpful?
What can we do to improve the information ?