Technical FAQs

Ask a Question

Can MA, MH, ME and MX breakers be backfed?

Yes, there are no restrictions for line or load connections. See Class 601 catalog for further clarification. If using ME or MX with Ground fault protection, please note proper orientation of the neutral CT is critical. See instruction bulletin for details.


CTA-ID : 2003889
Was this helpful?
What can we do to improve the information ?