Technical FAQs

Ask a Question

Can the 9037HG type float switch be used in a tank rated for 60 PSI?

The std switch can with stand up to 50 psi @ 220 degrees F.


CTA-ID : 2003888
Was this helpful?
What can we do to improve the information ?