Technical FAQs

Ask a Question

How much side gutter space is in an MA1000R with an MAL circuit breaker installed?

There is 5.56`` on either side of the MAL circuit breaker to the side wall of the enclosure.
CAUTION: If used, the SN1000MA neutral assembly will be mounted in the right side gutter, to the right side of the MAL circuit breaker. This will take up any useable wiring gutter available on the right side of the circuit breaker.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2003634
Was this helpful?
What can we do to improve the information ?