Technical FAQs

Ask a Question

Some of Square D`s larger low voltage dry type distribution transformers have a barrier inside. Is that a shipping brace that should be removed?

The is a barrier is an integral part of the transformer`s design. Do not remove it.

CTA-ID : 2004438
Was this helpful?
What can we do to improve the information ?