Technical FAQs

Ask a Question

Is there a picture showing forms N3 & N5 on a 9038AW1?

No pictures available.
N3 is internal to the switch and is the addition of a manual lead & lag selector toggle switch .
N5 is the addition of a third warning signal switch (single pole) It consists of a slotted cast metal plate internal to switch mechanism .

Note: The N5 is a basic 9007 AO1 snap switch....Use the picture for this if you wants...




CTA-ID : 2003870
Was this helpful?
What can we do to improve the information ?