Technical FAQs

Ask a Question

What is the external reset for an 8539SGA54?

The complete, door mounted, external reset mechanism assembly requires the following parts:
(1) -30019-113-66, Reset sub-assembly.
(1) 30019-121-01, Ring nut.
(1) 29206-30700, Gasket.




CTA-ID : 2004426
Was this helpful?
What can we do to improve the information ?