Technical FAQs

Ask a Question

Can you order the replacement GTO 52915-029-50 for 8804?

No. There is a very limited supply of these parts. The only way to get this Frame B size drive repaired is to send it into the repair depot.

This is also the same for the Frame A size Omegapaks which do not have GTOs available either for customer order and require return to depot for repair.

A frame = 1-20hp @ 460v (25hp variable torque)
B frame = 25-40hp @ 460v (50hp variable torque)

Can go through a local distributor to have unit sent in for repair.  Can locate a local distributor at at attached URL:

CTA-ID : 2000300
Was this helpful?
What can we do to improve the information ?