Technical FAQs

Ask a Question

Where is the ground fault push to test feature on the GC200 relay ground fault system?

The GCDSP display has a trip test and no trip test as a menu option under the relay test mode.

An auxiliary trip input (remote trip test) can be wired to terminals 21 and 25 on the relay.

On some sensors an auxiliary test input can be wired through the sensor.

A remote reset can be wired to terminals 19 and 25 on the relay.


CTA-ID : 2004162
Was this helpful?
What can we do to improve the information ?