Technical FAQs

Ask a Question

Can a KAL36250 be mounted in a KA225S circuit breaker enclosure?

No, the KA225S is restricted to 225 ampere maximum, due to wire bending space restrictions. Consider using LA400S.


CTA-ID : 2004156
Was this helpful?
What can we do to improve the information ?