Technical FAQs

Ask a Question

Is the KAD1PZ padlockable handle?

This handle assembly has the following features:

Size = 60 x 60mm
Color = Black
Padlockable = Yes
Mounting = Single hole (22.5mm)
Style = Selector switch
Protection = IP65 (gasket included)
Switches (for use with) = VN12, VN20, V0, V01, V02, V1, V2
Shaft Diameter = 6mm


CTA-ID : 2002715
Was this helpful?
What can we do to improve the information ?