Technical FAQs

Ask a Question

What is the Neutral Assembly for a HU361, Series F05 safety switch?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
Use SN03 or SN03C. The SN03 will accept aluminum or copper conductors. The SN03C will accept copper conductors only.


CTA-ID : 2002933
Was this helpful?
What can we do to improve the information ?