Technical FAQs

Ask a Question

What are part numbers 80110-792-01 and 24303-63190?

The 80110-792-01 is a closing plate and the 24303-63190 is a retractable pin rivet. These components are part of the NQODSF sub-feed breaker kit used on 400A and 600A NQOD interiors. The NQODSF is designed to accommodate (2) sub-feed breakers. The closing plate is used to cover the deadfront opening when only (1) sub-feed breaker is called for.

Revised 3/10/04



CTA-ID : 2002697
Was this helpful?
What can we do to improve the information ?