Technical FAQs

Ask a Question

What hubs are used with a HU363CS safety switch?

No hubs are required to be purchased separately. This cast aluminum safety switch is provided with a drilled and tapped 1 1/2`` conduit entry in both endwalls. Reducer bushings for use with 1 1/4`` and 1`` conduit are also provided. This information is also valid for H361CS, HU361CS, H362CS, HU362CS and H363CS.


CTA-ID : 2003129
Was this helpful?
What can we do to improve the information ?