Technical FAQs

Ask a Question

What is a BX30RFT?

This is a number that is on the Box Label as the Box Catalog Number. For instance, the Interior Label, located on the actual interior of a QO1816M150FTRB, will note the catalog number of the load center and state ``Use in Box Number BX30RFT``. The BX30RFT is not a system reckognized number. It cannot be ordered and cannot be used to identify the load center. The actual load center catalog number will be noted on the Interior Label mentioned above.

CTA-ID : 2002927
Was this helpful?
What can we do to improve the information ?