Technical FAQs

Ask a Question

What is the black lever on an integral starter which is located beneath the red operating knob?

Door interlock mechanism which prevents the opening of the enclosure door when Integral is flush mounted unless the operating knob is in the off position.


CTA-ID : 2003111
Was this helpful?
What can we do to improve the information ?