Technical FAQs

Ask a Question

Can you supply 120V single phase into the LH4N and bring it out to a 3 phase motor?

The unit has 1 SCR on phase 1. He needs to supply 208/240 single phase to the line side and bring the wires in on L1 and L2.

Please clarify the response. It does not answer the question. The answer is no. Single phase power can not run a 3 phase motor.


CTA-ID : 7513
Was this helpful?
What can we do to improve the information ?