Technical FAQs

Ask a Question

Do we show a 24 vdc rating on the 9007 limit switches?

No. All 9007 limit switches except the ML, MS, T and FT have DC data published. Tables begin at 125VDC which implies that they may be used below 125Vdc. One DC limitation is very low current , when used on a conventional set of contacts, will cause oxidization, resulting in contact failure. This is true where there is not sufficient arcing during contact opening and closure to burn off the corrosion.



CTA-ID : 2002062
Was this helpful?
What can we do to improve the information ?